eo_logo
 
Product added to cart
Building a Mach-Zehnder Interferometer

Building a Mach-Zehnder Interferometer

What is a Mach-Zehnder Interferometer?

Mach-Zehnder interferometers are simple interferometric instruments that measure the relative phase shift between two collimated light beams. This phase shift can be used to determine small displacements, the transmitted wavefront error of transmissive optics, the refractive index of transparent materials, air flow in wind tunnels, and more.

Mach-Zehnder interferometers consist of a coherent light source like a laser, two beamsplitters, and two mirrors (Figure 1 and Figure 2). First, the light source is split into two paths using the first beamsplitter. The two beams each have the same optical path length, which is the distance traveled multiplied by the refractive index of the media they travel through. Each beam reflects off of a mirror and is recombined by the second beamsplitter. If there is a difference in the optical path lengths of the two beams that is less than the coherence length of the light source, interference fringes will be generated. Because the coherence length of a source can be extremely short, precision components and alignment are crucial. A sample can be measured by being placed in one of the beam paths. The resulting optical path length difference can be measured by observing the change in the interference fringes.

Typical optical schematic of a Mach-Zehnder interferometer
Figure 1: Typical optical schematic of a Mach-Zehnder interferometer
Assembled tabletop Mach-Zehnder interferometer system constructed out of off-the-shelf components from Edmund Optics
Figure 2: Assembled tabletop Mach-Zehnder interferometer system constructed out of off-the-shelf components from Edmund Optics®

Assembling System using Off-the-Shelf Components from Edmund Optics®

A system like the one shown in Figure 2 can be assembled by following the guide below. \

Sub-Assemblies

Each optical sub-assembly can be added to a table-top breadboard and easily slid along the optical axis via optical rails. The small linear motion stage placed on the carrier of the optical rail makes it easy to make fine adjustments in the optical axis direction or the orthogonal direction.

Optical Base

Stock # Description Quantity
#54641 600mm x 300mm, Breadboard 1
#54929 500mm Length, Compact Optical Rail 2

Light Source

Stock # Description Quantity
#86848 Coherent® StingRay™ Laser Diode Module 1231490 | 520nm, 5mW 1
#59099 5V Universal Power Supply 1
#18291 E-Series 19.1mm ID Adapter 1
#15866 25.0/25.4mm Optic Dia., E-Series Kinematic Mount 1
#59760 63.5mm Length, M6 Stud, Steel Post 1
#58973 76.2mm Length, M6 Thread, Post Holder 1
#58992 Post Collar 1
#16714 Dovetail Stage, 30mm SQ, Metric 1
#11164 30mm Length x 35mm Width, Compact Carrier 1
Light source sub-assembly
Figure 3: Light source sub-assembly

Iris Diaphragm

Stock # Description Quantity
#53914 30.8mm Outer Diameter, Mounted Iris Diaphragm 2
#58963 2.5" Length, 8-32 Stud, Steel Post 2
#58973 76.2mm Length, M6 Thread, Post Holder 2
#58992 Post Collar 2
#16714 Dovetail Stage, 30mm SQ, Metric 2
#11164 30mm Length x 35mm Width, Compact Carrier 2
Iris diaphragm sub-assembly
Figure 4: Iris diaphragm sub-assembly

Plano-Concave Lens Mount

Stock # Description Quantity
#64552 6.0mm Optic Dia., Optic Mount 1
#48690 6mm Diameter x -15 FL, VIS 0° Coated, Plano-Concave Lens 1
#59760 63.5mm Length, M6 Stud, Steel Post 1
#58973 76.2mm Length, M6 Thread, Post Holder 1
#58992 Post Collar 1
#16714 Dovetail Stage, 30mm SQ, Metric 1
#11164 30mm Length x 35mm Width, Compact Carrier 1
Plano-concave lens mount sub-assembly
Figure 5: Plano-concave lens mount sub-assembly

Plano-Convex Lens Mount

Stock # Description Quantity
#13787 25.0/25.4mm Optic Dia., SM1 Thin Mount, M4 1
#62573 25.4mm Dia. x 76.2mm FL, VIS 0° Coated, Plano-Convex Lens 1
#58953 63.5mm Length, M4 Stud, Steel Post 1
#58973 76.2mm Length, M6 Thread, Post Holder 1
#58992 Post Collar 1
#16714 Dovetail Stage, 30mm SQ, Metric 1
#11164 30mm Length x 35mm Width, Compact Carrier 1
Plano-convex lens mount sub-assembly
Figure 6: Plano-convex lens mount sub-assembly

Projection Lens Mount

Stock # Description Quantity
#13787 25.0/25.4mm Optic Dia., SM1 Thin Mount, M4 1
#47917 25mm Dia. x -25mm FL, VIS 0° Coated, Double-Concave Lens 1
#58953 63.5mm Length, M4 Stud, Steel Post 1
#58973 76.2mm Length, M6 Thread, Post Holder 1
#58992 Post Collar 1
#16714 Dovetail Stage, 30mm SQ, Metric 1
#11164 30mm Length x 35mm Width, Compact Carrier 1
Projection lens mount sub-assembly
Figure 7: Projection lens mount sub-assembly

Gimbal Mount with Mirror (2set)

Stock # Description Quantity
#54999 25.0/25.4mm Optic Dia., Precision Gimbal Mount 2
#64015 25mm Diameter Enhanced Aluminum Coated, λ/10 Mirror 2
#59759 50.8mm Length, M6 Stud, Steel Post 2
#58972 50.8mm Length, M6 Thread, Post Holder 2
#58992 Post Collar 2
#66393 30mm, Side Drive, Standard Top, 0.5" Travel, Metric Micrometer 2
#11164 30mm Length x 35mm Width, Compact Carrier 2
Gimbal mount with mirror sub-assembly
Figure 8: Gimbal mount with mirror sub-assembly

Gimbal Mount with Beamsplitter (2set)

Stock # Description Quantity
#54999 25.0/25.4mm Optic Dia., Precision Gimbal Mount 2
#34413 25mm Diameter 50R/50T, VIS Wedged Plate Beamsplitter 2
#59759 50.8mm Length, M6 Stud, Steel Post 2
#58972 50.8mm Length, M6 Thread, Post Holder 2
#58992 Post Collar 2
#66393 30mm, Side Drive, Standard Top, 0.5" Travel, Metric Micrometer 2
#11164 30mm Length x 35mm Width, Compact Carrier 2
Gimbal mount with beamsplitter sub-assembly
Figure 9: Gimbal mount with beamsplitter sub-assembly

Full Parts List

Stock # Description Quantity
#54641 600mm x 300mm, Breadboard 1
#54929 500mm Length, Compact Optical Rail 2
#11164 30mm Length x 35mm Width, Compact Carrier 10
#16714 Dovetail Stage, 30mm SQ, Metric 6
#66393 30mm, Side Drive, Standard Top, 0.5" Travel, Metric Micrometer 4
#58972 50.8mm Length, M6 Thread, Post Holder 4
#58973 76.2mm Length, M6 Thread, Post Holder 6
#58992 Post Collar 10
#59760 63.5mm Length, M6 Stud, Steel Post 2
#58953 63.5mm Length, M4 Stud, Steel Post 2
#59759 50.8mm Length, M6 Stud, Steel Post 4
#58963 2.5" Length, 8-32 Stud, Steel Post 2
#86848 Coherent® StingRay™ Laser Diode Module 1231490 | 520nm, 5mW 1
#59099 5V Universal Power Supply 1
#15866 25.0/25.4mm Optic Dia., E-Series Kinematic Mount 1
#18291 E-Series 19.1mm ID Adapter 1
#53914 30.8mm Outer Diameter, Mounted Iris Diaphragm 2
#64552 6.0mm Optic Dia., Optic Mount 1
#48690 6mm Diameter x -15 FL, VIS 0° Coated, Plano-Concave Lens 1
#13787 25.0/25.4mm Optic Dia., SM1 Thin Mount, M4 2
#62573 25.4mm Dia. x 76.2mm FL, VIS 0° Coated, Plano-Convex Lens 1
#47917 25mm Dia. x -25mm FL, VIS 0° Coated, Double-Concave Lens 1
#54999 25.0/25.4mm Optic Dia., Precision Gimbal Mount 4
#64015 25mm Diameter Enhanced Aluminum Coated, λ/10 Mirror 2
#34413 25mm Diameter 50R/50T, VIS Wedged Plate Beamsplitter 2

Aligning a Mach-Zehnder Interferometer

The laser, iris, and lenses must be aligned to the same optical axis. Ideally, the optical axis of these components should not change even if they are translated on the optical rail. A stage installed on the optical rail carrier allows for horizontal movement perpendicular to the direction of the rail.

  1. Installing the Laser Module
    • Fix the laser module (diameter Φ19.1mm) to #15866 using the adapter (#18291).
    • This makes it easy to adjust the laser angle.
    • Adjust the angle of the mount so that the laser beam is parallel to the optical rail.
    Installing the laser module
    Installing the laser module
    Figure 10: Installing the laser module
  2. Aligning the Laser's Optical Axis
    • Use the iris sub-assembly to keep the center of the optical axis of all components of the system constant.
    • Direct the laser onto the center of the iris.
    • Slide the iris down the optical rail while making adjustments to the kinematic mount to keep the laser centered on the iris throughout the whole range.
    Aligning the laser's optical axis
    Figure 11: Aligning the laser's optical axis
  3. Aligning the Plano-Convex Lens' Optical Axis
    • Adjust the optical axis of a plano-convex lens with the long focal length while sliding the lens unit left and right.
    • Use the post to adjust the height of the lens and use the dovetail stage to adjust the optical axis in the perpendicular direction.
    Aligning the optical axis of the plano-convex lens with the long focal length
    Figure 12: Aligning the optical axis of the plano-convex lens with the long focal length
  4. Aligning the Plano-Concave Lens' Optical Axis
    • Place a plano-concave lens with a short focal length in the optical path.
    • Adjust the optical axis while sliding the lens unit left and right.
    • Use the post to adjust the height of the lens and use the dovetail stage to adjust the optical axis in the perpendicular direction.
    Aligning the optical axis of the plano-concave lens with the short focal length
    Figure 13: Aligning the optical axis of the plano-concave lens with the short focal length
  5. Positioning Lenses to Form Beam Expander
    • The two lenses should be separated by the sum of their focal lengths. In this case, the separation should be 76.2mm – 25mm = 51.2mm.
    • To learn more about pairing lenses to expand the diameter of a beam to a desired size, please visit our How to Design Your Own Beam Expander Using Stock Optics application note.
    • Selecting coated lenses with low reflectance is important for avoiding stray light.
    Positioning the two lens sub-assemblies in front of the iris to form a beam expander
    Figure 14: Positioning the two lens sub-assemblies in front of the iris to form a beam expander
  6. Aligning Mirrors and Beamsplitters
    • The two optical path lengths must be equal (or nearly equal) and the final beams must overlap to obtain fringes.
    • A beamsplitter is placed in position A to split the laser into two paths and another beamsplitter is placed at D to recombine the beams.
    • Adjust distances so that the optical path lengths of A-B-D and A-C-D are the same.
    • Care must be taken to prevent the edges of the mirror/beamsplitter mounts from blocking the beam.
    • The beam transmitted through D must overlap with the beam reflected at D.
    • Adjust the mirror positions and angles so the two beams overlap right after D as well as further down the rail past D (Figure 15).
    Aligning the mirrors and beamsplitters
    Figure 15: Aligning the mirrors and beamsplitters
  7. Check for Interference Fringes
    • Adding a magnifying lens after D can make it easier to identify fringes.
    • The stage position on the optical rail and alignment of other components may need to be fine-tuned to obtain fringes
    Final Mach-Zehnder interferometer setup constructed out of off-the-shelf components
    Figure 16: Final Mach-Zehnder interferometer setup constructed out of off-the-shelf components

More Resources

這項內容對您是否實用?

 

 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin
This site is protected by VikingCloud's Trusted Commerce program