Product added to cart
All Press Releases

Mount Cylinder Lenses and Non-Standard Sized Components with the New E-Series Kinematic Mounts

6/28/2022, Barrington, NJ USA   —

Edmund Optics®, a leading global manufacturer and supplier of optical components, has expanded its extensive inventory by increasing its offering of optomechanical mounts. This product expansion includes the E-Series Adjustable Size Kinematic Optical Mounts which are ideal for mounting a wide range of round, rectangular, and square optical components, including round and rectangular cylinder lenses. These kinematic adjustment mounts are essential for integrating non-standard sized optical components in both experimental applications and OEM systems.

The E-Series Adjustable Size Kinematic Optical Mounts feature wide clear aperture for compatibility with both reflective optics and transmissive optics such as mirrors, beamsplitters, filters, and cylinder lenses. The M6 x 0.25 (101.6 TPI) adjustment screws can be driven by hand or by 2mm sized Allen key for fine adjustment and alignment of optical tip and tilt (±3.5°). Adjustment screws knobs are removable for more compact space-constrained applications. These mounts are compatible with M4, 8-32, and M6 x 1.0 hardware for mounting versatility and compatibility with TECHSPEC® Metric Stainless Steel Mounting Posts and Pedestal Posts.

To view these, and many more exciting, new products offered by Edmund Optics, visit the new products page at www.edmundoptics.com.

About Edmund Optics:

Edmund Optics® is a leading global supplier of optics, imaging, and photonics technology that has served a variety of markets including Life Sciences, Biomedical, Industrial Inspection, Semiconductor, R&D, and Defense since 1942. The company designs and manufactures a wide array of optical components, multi-element lenses, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of stock and custom products. Operating in more than a dozen major facilities around the globe, Edmund Optics employs just over 1,100 employees and continues to expand. Customers can purchase items by calling 1-800-363-1992, via the catalog, or on the website at www.edmundoptics.com.

 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin