Edmund Optics® (EO), the premier provider of optical components, announced today that it was awarded a Silver Level Award for its TECHSPEC® Titan TL Telecentric Lenses. These lenses were recognized among the best in the industry by the judges of the Vision Systems Design 2017 Innovators Awards program.
The TECHSPEC® Titan TL Telecentric Lenses are versatile lenses designed for machine vision systems and metrology applications that require a wide field of view. Applications include automotive and electronic inspection, measurement and gauging.
Lenses feature large maximum sensor formats
TECHSPEC® Titan TL Telecentric Lenses have low distortion and exhibit less than 0.1° telecentricity for optimal accuracy. The lenses feature large maximum sensor formats of 1⁄1.8”, 2⁄3”, 1” and 4⁄3”. Sixteen models are offered in working distances from 111mm to 374mm with a variety of magnification options. A convenient rear filter holder on the back of the lenses allows for easy filter integration. An integrated mounting flange on our 118mm, 182mm and 242mm FOV versions lets users easily secure each lens without an additional mount and provides a convenient reference plane. Shims are included to provide adjustment for camera sensor location variations. An adjustable iris and a three set screw lens mount provides simple rotational alignment to the camera. The RoHS compliant lenses feature a λ/4 at 520nm MgF2 anti-reflection coatings. TECHSPEC® Titan TL Telecentric Lenses are in-stock and available for immediate delivery for fast turnaround and excellent value.
About The Vision Systems Design 2017 Innovators Awards program
The Vision Systems Design 2017 Innovators Awards program reviewed and recognized the most innovative products and services in the vision and image processing industry. Honorees were announced at Automate 2017 held in Chicago, Illinois, USA. Criteria used in the Innovators Awards ranking included: originality, innovation; impact on designers, systems integrators and end-users; fulfilling a need in the market that hasn’t been addressed, leveraging a novel technology, and increasing productivity.
About Edmund Optics:
Edmund Optics® is a leading supplier of optics, imaging, and photonics technology for the Life Sciences, Biomedical, Semiconductor, R&D, and Defense markets around the globe. Edmund Optics designs and manufactures a wide array of multi-element lenses, lens coatings, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of both stock and custom products. Edmund Optics’ state-of-the-art manufacturing capabilities, combined with its global distribution network, has earned it the position of the world’s largest supplier of off-the-shelf optical components. Customers can purchase items by calling 1-800-363-1992, via the catalog or the website at www.edmundoptics.com.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information