test_cookieUsed to check if the user's browser supports cookies.
最大存储时长: 1 天类别: HTTP Cookie
rc::aThis cookie is used to distinguish between humans and bots. This is beneficial for the website, in order to make valid reports on the use of their website.
最大存储时长: 永久类别: HTML 本地存储
rc::cThis cookie is used to distinguish between humans and bots.
__cf_bm [x3]This cookie is used to distinguish between humans and bots. This is beneficial for the website, in order to make valid reports on the use of their website.
AWSALB [x2]Registers which server-cluster is serving the visitor. This is used in context with load balancing, in order to optimize user experience.
最大存储时长: 7 天类别: HTTP Cookie
AWSALBCORS [x2]Registers which server-cluster is serving the visitor. This is used in context with load balancing, in order to optimize user experience.
_conv_rThis cookie is used as a referral-cookie that stores the visitor’s profile – the cookie is overwritten when the visitor re-enters the website and new information on the visitor is collected and stored.
最大存储时长: 临时类别: HTTP Cookie
_conv_sThis cookie contains an ID string on the current session. This contains non-personal information on what subpages the visitor enters – this information is used to optimize the visitor's experience.
最大存储时长: 1 天类别: HTTP Cookie
_conv_vThis cookie is used to identify the frequency of visits and how long the visitor is on the website. The cookie is also used to determine how many and which subpages the visitor visits on a website – this information can be used by the website to optimize the domain and its subpages.
conv_randThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
最大存储时长: 永久类别: HTML 本地存储
_conv_sptestThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
_ga [x2]Used to send data to Google Analytics about the visitor's device and behavior. Tracks the visitor across devices and marketing channels.
最大存储时长: 25 月类别: HTTP Cookie
_ga_# [x2]Used to send data to Google Analytics about the visitor's device and behavior. Tracks the visitor across devices and marketing channels.
最大存储时长: 25 月类别: HTTP Cookie
_gcl_au [x2]Used by Google AdSense for experimenting with advertisement efficiency across websites using their services.
最大存储时长: 3 月类别: HTTP Cookie
IDE待定
最大存储时长: 400 天类别: HTTP Cookie
NIDRegisters a unique ID that identifies a returning user's device. The ID is used for targeted ads.
最大存储时长: 6 月类别: HTTP Cookie
pagead/1p-user-list/#Tracks if the user has shown interest in specific products or events across multiple websites and detects how the user navigates between sites. This is used for measurement of advertisement efforts and facilitates payment of referral-fees between websites.
Multi-Axis Translation Stage Configurations: Part II: X-Y-Z Setup
Continuing from where Part I: X-Y Setup ends, learn how to add a Z-axis to an existing X-Y configuration to achieve three degrees of freedom. Use this easy step-by-step video to help you create a system that provides finer resolution than just moving a post up and down. Randall Hinton, Solutions Engineer, demonstrates how to assemble a three-axis (X-Y-Z) configuration using Edmund Optics' TECHSPEC® Single Axis Crossed Roller Translation Stages in part II of this informative video series.
Hi, my name is Randall, a Solutions Engineer at Edmund Optics. In Part 1, I took just a couple of minutes to assemble an X-Y Translation Stage system allowing for repeatable adjustments and precise alignment in two directions. Many applications require adjustment in the Z direction, rather than just moving a post up and down. Today, I will add a Z-Axis to our assembled X-Y configuration, creating an X-Y-Z setup. This is a bit trickier because of the way the micrometer is mounted onto the stage. The positioning of the micrometer causes the load to be supported by the spring tension. In order to alleviate this, I will show you how to remove the micrometer, re-attach it to an existing X-Y configuration, with the addition of a Z bracket. In addition to the X-Y setup we configured in Part 1, we need the following mechanical components. 40mm, Side Drive, Solid Top Metric Stage. 40mm Z bracket. 2mm, metric Allen Wrench and 0.05-inch English Allen Wrench. Let's start. Step 1: Align the 4 M3 counterbored holes in the Z-Axis bracket to the corresponding holes in the top plate of the 40mm stage. Step 2: Now using the included M3 Socket Head Cap Screws and the 2.5mm metric Allen Wrench, fasten down the bracket to the top plate. Step 3: Tighten the clamp screw and secure the stage. Next, loosen the screws securing the micrometer head with the 0.05-inch English Allen Wrench and remove the micrometer head. Step 4: Now remove the micrometer base and the micrometer stopper with the 2mm Allen Wrench. Now removing the stopper. Speeding up the video. Next, remove the clamp screws with a Phillips-head screwdriver, removing the clamp screw and the clamp plate. Step 5: Attach this stage to the Z-Axis bracket. First, using a 2.5mm metric Allen Wrench and the included M3 Socket Head Cap Screws, secure the two screws on the upper side. Move the stage by hand and then secure the screws on the lower side. Next, move the stage to an adequate position and tighten the clamp screw over the clamp plate. Then secure the clamp screws. Step 7: Attach the micrometer stopper, then the micrometer base. You may note that the attached position and the direction differ from the previous position and direction of the original stage. Be sure to tighten the screws securely. Step 8: Insert the micrometer head into the micrometer base. Insert the micrometer head all the way in securely. If it does not go in all the way, move the stage or adjust the micrometer. Be sure to rotate the head so that the dial on the micrometer head can be seen clearly, securing it with a set screw. Note that the attached position and direction differ from the previous position and direction of the original configuration. As you can see, you have now created a complete X-Y-Z Axis Translation Stage system. You can now make repeatable, precise movements in three dimensions after a little assembly of our standard components. I hope you have enjoyed Part 1 and Part 2 of this video series. Remember, if you have any further questions or would like to discuss your next application, feel free to contact Edmund Optics Tech Support today.
Please select your shipping country to view the most accurate inventory information, and to determine the correct Edmund Optics sales office for your order.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information