test_cookieUsed to check if the user's browser supports cookies.
最大存储时长: 1 天类别: HTTP Cookie
rc::aThis cookie is used to distinguish between humans and bots. This is beneficial for the website, in order to make valid reports on the use of their website.
最大存储时长: 永久类别: HTML 本地存储
rc::cThis cookie is used to distinguish between humans and bots.
__cf_bm [x3]This cookie is used to distinguish between humans and bots. This is beneficial for the website, in order to make valid reports on the use of their website.
AWSALB [x2]Registers which server-cluster is serving the visitor. This is used in context with load balancing, in order to optimize user experience.
最大存储时长: 7 天类别: HTTP Cookie
AWSALBCORS [x2]Registers which server-cluster is serving the visitor. This is used in context with load balancing, in order to optimize user experience.
_conv_rThis cookie is used as a referral-cookie that stores the visitor’s profile – the cookie is overwritten when the visitor re-enters the website and new information on the visitor is collected and stored.
最大存储时长: 临时类别: HTTP Cookie
_conv_sThis cookie contains an ID string on the current session. This contains non-personal information on what subpages the visitor enters – this information is used to optimize the visitor's experience.
最大存储时长: 1 天类别: HTTP Cookie
_conv_vThis cookie is used to identify the frequency of visits and how long the visitor is on the website. The cookie is also used to determine how many and which subpages the visitor visits on a website – this information can be used by the website to optimize the domain and its subpages.
conv_randThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
最大存储时长: 永久类别: HTML 本地存储
_conv_sptestThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
_ga [x2]Used to send data to Google Analytics about the visitor's device and behavior. Tracks the visitor across devices and marketing channels.
最大存储时长: 25 月类别: HTTP Cookie
_ga_# [x2]Used to send data to Google Analytics about the visitor's device and behavior. Tracks the visitor across devices and marketing channels.
最大存储时长: 25 月类别: HTTP Cookie
_gcl_au [x2]Used by Google AdSense for experimenting with advertisement efficiency across websites using their services.
最大存储时长: 3 月类别: HTTP Cookie
IDE待定
最大存储时长: 400 天类别: HTTP Cookie
NIDRegisters a unique ID that identifies a returning user's device. The ID is used for targeted ads.
最大存储时长: 6 月类别: HTTP Cookie
pagead/1p-user-list/#Tracks if the user has shown interest in specific products or events across multiple websites and detects how the user navigates between sites. This is used for measurement of advertisement efforts and facilitates payment of referral-fees between websites.
How to Determine Magnification of an Optical Lens Setup
When doing basic imaging, how do you determine the magnification an optical lens will provide? Monica Rainey, Optical Engineer, demonstrates and explains how to calculate magnification with a simple setup and corrects some common misconceptions.
Hi, I am Monica, an Optical Engineer here at Edmund Optics. Today, I want to talk about one of the common questions we get from customers. When doing basic imaging, how do you determine the magnification a single lens will provide? A common misconception is that magnification is a property of the lens itself, when in reality, it is a result of how the system is laid out. To illustrate this point, we've setup a simple imaging system. Here, we have an object, single lens and image plane. With this system, we know we can apply the imaging equation shown here. We recall that n prime and n both equal 1 since we are in air and we know z is negative according to our sign convention since we measure it from right to left. For further detail on the imaging equation, please watch the video linked in the text below. The magnification can be found by taking the ratio of the image distance to the object distance. A negative magnification indicates the image will be inverted. A positive magnification indicates the image will be upright. Since we have a negative distance and a positive distance for our setup here, we have an inverted image, which you can see here. This equation can be solved to find the magnification of a given system, or to find the object and image distance required to achieve the desired magnification. We can also use this equation, along with the imaging equation, to determine the focal length of a lens needed to meet the requirements of a system. You can see these equations are tied to each other, so it is not possible to independently select object distance, image distance and magnification. Since we now know that magnification is the ratio of image to object distance, we can determine where our lens need to be if we want to focus the source down to be smaller or expanded to be larger. If you want to make your source or object larger, with a magnification greater than 1, the lens must be closer to your object than the image, since image distance must be greater than your object distance. However, recall from our previous video, that if your object is closer to the lens than its focal length, an image will not form. If you want to focus your object down to be smaller, with a magnification less than 1, the lens must be closer to your image than the object since the object distance must be greater than the image distance. Often times, we are also asked about the magnifying power of a lens. For example, you might need 3x magnification for an inspection application. Again, magnification is not a property of the lens itself but of how it is used in the system. However, there is an easy rule of thumb to help you determine the magnification for a hand-held magnifier. Magnifying power can be determined when the lens is at the near point of your eye, which is about 10 inches or 250mm in front of the eye. To find the approximate magnifying power, divide the 250mm near point length by the focal length of the lens in mm as shown in this equation. For example, a 25mm focal length lens provides magnifying power of approximately 10x when held near the eye. However, remember that this is only valid when using a lens with the human eye as the magnifier, not in an optical bench setup. I hope this helps you in understanding magnification. You can browse more of our technical application notes and videos to learn more key concepts and find answers to common questions on our website.
Please select your shipping country to view the most accurate inventory information, and to determine the correct Edmund Optics sales office for your order.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information