Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
我们不使用这种类别的 cookie
Polarization refers to the direction with which the electric field of light waves oscillate, which is perpendicular to the direction of propagation. Light waves can be linearly, circularly, elliptically, or randomly polarized. For more information about polarization read Introduction to Polarization.
Laser sources may be polarized due to anisotropy (a material property that is different in different directions) in the laser gain material, directionally dependent polarization losses in the laser resonator, or the use of birefringent optical materials. Some laser sources are unpolarized (e.g. fiber lasers). The polarization state of a laser can also be used to reduce unwanted and potentially dangerous reflection from high-power sources as some materials reflect or absorb light in certain polarizations states over others.
Many laser applications including some interferometry, optical amplification and modulation, nonlinear frequency conversion, and incoherent and coherent polarization beam combining (polarization coupling), depend on the state of polarization in order to function.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information