test_cookieUsed to check if the user's browser supports cookies.
最大存储时长: 1 天类别: HTTP Cookie
rc::aThis cookie is used to distinguish between humans and bots. This is beneficial for the website, in order to make valid reports on the use of their website.
最大存储时长: 永久类别: HTML 本地存储
rc::cThis cookie is used to distinguish between humans and bots.
__cf_bm [x3]This cookie is used to distinguish between humans and bots. This is beneficial for the website, in order to make valid reports on the use of their website.
AWSALB [x2]Registers which server-cluster is serving the visitor. This is used in context with load balancing, in order to optimize user experience.
最大存储时长: 7 天类别: HTTP Cookie
AWSALBCORS [x2]Registers which server-cluster is serving the visitor. This is used in context with load balancing, in order to optimize user experience.
_conv_rThis cookie is used as a referral-cookie that stores the visitor’s profile – the cookie is overwritten when the visitor re-enters the website and new information on the visitor is collected and stored.
最大存储时长: 临时类别: HTTP Cookie
_conv_sThis cookie contains an ID string on the current session. This contains non-personal information on what subpages the visitor enters – this information is used to optimize the visitor's experience.
最大存储时长: 1 天类别: HTTP Cookie
_conv_vThis cookie is used to identify the frequency of visits and how long the visitor is on the website. The cookie is also used to determine how many and which subpages the visitor visits on a website – this information can be used by the website to optimize the domain and its subpages.
conv_randThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
最大存储时长: 永久类别: HTML 本地存储
_conv_sptestThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
_ga [x2]Used to send data to Google Analytics about the visitor's device and behavior. Tracks the visitor across devices and marketing channels.
最大存储时长: 25 月类别: HTTP Cookie
_ga_# [x2]Used to send data to Google Analytics about the visitor's device and behavior. Tracks the visitor across devices and marketing channels.
最大存储时长: 25 月类别: HTTP Cookie
_gcl_au [x2]Used by Google AdSense for experimenting with advertisement efficiency across websites using their services.
最大存储时长: 3 月类别: HTTP Cookie
IDE待定
最大存储时长: 400 天类别: HTTP Cookie
NIDRegisters a unique ID that identifies a returning user's device. The ID is used for targeted ads.
最大存储时长: 6 月类别: HTTP Cookie
pagead/1p-user-list/#Tracks if the user has shown interest in specific products or events across multiple websites and detects how the user navigates between sites. This is used for measurement of advertisement efforts and facilitates payment of referral-fees between websites.
Powered by Edmund Optics: High Performance Sensing by Ocular Robotics
Learn how Edmund Optics can take you from design to prototype to volume production in this high performance sensing demo from Ocular Robotics. Demo highlights a 3D LIDAR system and security application both powered by Edmund Optics optical components. How can Edmund Optics help you? http://www.edmundoptics.com/prototyping
So, what we have got is a pair of ocular robotics systems. Right down here is called a camera system so it is building up a panorama using high pointing accuracy from whatever I give this, or you can just grab the images, drop them straight into the matrix. We don't need to do any image matching or anything like that. At the top here, we've got a 3D wide-eye system so that is producing the point cloud you see up in this section here, so that is doing a full scan of the whole area on frame. Down here you can see panorama, images coming up, depositing up to build ourselves a full shot and this lovely shot of our camera man right in the middle. Once we have got these two pieces of data we can actually combine them together, so we have very good information about the position where the images were taken, and very good information about the laser information. That gives us the ability to combine both of them and produce an RGB 3D point cloud. So that enables us to have both structure and color and texture information about specs. So, you can see here is the marching stand behind us colored in in red, after that we have got some more Northrop Grumman stuff so that is looking over in that direction. But you can see this is not just 3D data, you actually have got the color, and you've got the texture of the carpet, the texture of the floor in there. So that is the first demo we are running for you today. The second demo we are running for you is a basic security stall application just using the camera system. So, on this demo we are revisiting six target locations, two of them static. So, you can see we are actually revisiting this location to fix the level accuracy. You can actually see that image does not move at all. Simultaneously, updating static locations, we can also move our field of view. So, we can scan up and down, get multiple targets, scan across the sign up here, or even just look at something like a sign up here with varying camera exposure time as we expose the same location. So, we are effectively getting high dynamic range imagery. The Edmund Optics' material in this system: we have got five custom ground glass lenses installed to relay the optical information from the head down to the camera existing in the base. We also have Edmund's mirrors in both camera and the laser systems, and we used Edmund's off the shelf components to get to our prototyping stage, so we can produce a proof of concept of our camera system with adequate optical performance, but then for our full-on retail systems we are using all custom ground, custom design lenses.
Please select your shipping country to view the most accurate inventory information, and to determine the correct Edmund Optics sales office for your order.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information