Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
An indication of the peak-to-valley flatness of a surface given in terms of waves (a multiple or part of a reference wavelength). For example, a specification of 1/4 wave means that the flatness of the surface deviates by one quarter of the wavelength used to test the surface. If the wavelength was 550nm, the flatness would be held to within 140nm in order to produce a surface accuracy of 1/4 wave. Also given in RMS (root mean squared) where the peak-to-valley values are squared and then the square root is taken of their mean.
See also Reference Wavelength
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information