eo_logo
 
Product added to cart

Optical Fiber

A type of optic comprised of a core surrounded by a relatively thin cladding layer of lower index material. This geometry causes internal reflection of light inside the fiber and defines the maximum angles accepted by the fiber. An optical fiber emits into a cone of equal angle, not as a beam of light. Coherent fiber bundles can relay images from one end to the other; whereas, incoherent bundles are used for propagation of light alone.

See also Ball Lens , Bend Radius , Crosstalk , Buffer Material , Fiber Jacket , Decibel (dB) , Cladding , Packing Fraction

這項內容對您是否實用?
 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin
This site is protected by VikingCloud's Trusted Commerce program