eo_logo
 
Product added to cart

Modulation Transfer Function (MTF)

A measure of contrast as a function of spatial frequency. Defined as 100% at zero-frequency, MTF continuously declines with increasing spatial frequency to zero contrast at a theoretical maximum resolution frequency defined by the diffraction limit of the optical system.

See also Diffraction Limit , Contrast , Resolution

這項內容對您是否實用?
 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin
This site is protected by VikingCloud's Trusted Commerce program