eo_logo
 
Product added to cart

Jitter

An imaging phenomenon that limits the accuracy of measurement to at least two pixel separations because signals impinging on the sensor may fall on a pixel or on the space between pixels. Statistically speaking, the latter case may cause a response in the pixel to the immediate left or the immediate right of the space. Due to the standard scan frequency of 60Hz, such a static image will exhibit jitter between the two pixels in question over time. 

See also Pixel

這項內容對您是否實用?
 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin
This site is protected by VikingCloud's Trusted Commerce program