eo_logo
 
Product added to cart

Glass Code

A reference code for a specific glass type that is represented by three digits, then a slash, then another three digits. It is always present in technical prints to indicate the specifications of the glass substrate used. The first three digits refer to the three numbers after the decimal in the glass' index of refraction. The second three digits refer to the first three significant digits in the glass' Abbe number. For instance, BK7, which has an index of refraction of 1.517 and an Abbe number of 64.2, has a glass code of 517/642. 

See also Abbe-Number , Angle of Incidence , Angle of Reflection , Index of Refraction (n) , Dispersion

這項內容對您是否實用?
 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin
This site is protected by VikingCloud's Trusted Commerce program