test_cookieUsed to check if the user's browser supports cookies.
最大存储时长: 1 天类别: HTTP Cookie
rc::aThis cookie is used to distinguish between humans and bots. This is beneficial for the website, in order to make valid reports on the use of their website.
最大存储时长: 永久类别: HTML 本地存储
rc::cThis cookie is used to distinguish between humans and bots.
__cf_bm [x3]This cookie is used to distinguish between humans and bots. This is beneficial for the website, in order to make valid reports on the use of their website.
AWSALB [x2]Registers which server-cluster is serving the visitor. This is used in context with load balancing, in order to optimize user experience.
最大存储时长: 7 天类别: HTTP Cookie
AWSALBCORS [x2]Registers which server-cluster is serving the visitor. This is used in context with load balancing, in order to optimize user experience.
_conv_rThis cookie is used as a referral-cookie that stores the visitor’s profile – the cookie is overwritten when the visitor re-enters the website and new information on the visitor is collected and stored.
最大存储时长: 临时类别: HTTP Cookie
_conv_sThis cookie contains an ID string on the current session. This contains non-personal information on what subpages the visitor enters – this information is used to optimize the visitor's experience.
最大存储时长: 1 天类别: HTTP Cookie
_conv_vThis cookie is used to identify the frequency of visits and how long the visitor is on the website. The cookie is also used to determine how many and which subpages the visitor visits on a website – this information can be used by the website to optimize the domain and its subpages.
conv_randThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
最大存储时长: 永久类别: HTML 本地存储
_conv_sptestThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
_ga [x2]Used to send data to Google Analytics about the visitor's device and behavior. Tracks the visitor across devices and marketing channels.
最大存储时长: 25 月类别: HTTP Cookie
_ga_# [x2]Used to send data to Google Analytics about the visitor's device and behavior. Tracks the visitor across devices and marketing channels.
最大存储时长: 25 月类别: HTTP Cookie
_gcl_au [x2]Used by Google AdSense for experimenting with advertisement efficiency across websites using their services.
最大存储时长: 3 月类别: HTTP Cookie
IDE待定
最大存储时长: 400 天类别: HTTP Cookie
NIDRegisters a unique ID that identifies a returning user's device. The ID is used for targeted ads.
最大存储时长: 6 月类别: HTTP Cookie
pagead/1p-user-list/#Tracks if the user has shown interest in specific products or events across multiple websites and detects how the user navigates between sites. This is used for measurement of advertisement efforts and facilitates payment of referral-fees between websites.
It seems like you are experiencing some temporally-localized interference. If you look at a short enough slice of time, the photodiode might pick up the constantly shifting course of constructive and destructive interference that is basically what its called speckle.
Laser Diode Modules have a fair amount of noise if you look on a very short time scale. The total noise is a combination from multiple sources including but not limited to power supply noise, mode hopping, thermal effects, and optical feedback. These noise sources can be severely reduced by using a low-noise power supply and a heat sink or preferably a Thermo-electrically cooled (TEC) laser. In order for a laser to have a perfectly consistent output even on that small of a time scale, the necessary controls need to be designed in from the ground up, which is generally not the case with laser diode modules.
Silicon detectors are typically used for detecting laser signals and converting the signal to a voltage differential. For an in-depth explanation on the use of our silicon detectors, as well as circuit diagram examples, view Basic Principles of Silicon Detectors.
Our TE cooled Spectrometers, like the one you have, are calibrated for wavelength and not irradiance. The curve seen in the software is basically counts versus wavelength. The y-axis (counts) ranges from 0 to 2 x 16-1M or 65535, which is dependent on integration time that the user is allowed to set via the included software. In order to calibrate the spectrometer, you need to use a calibrated light source. Out of the box, you will be able to measure transmittance/reflection measurements but, again, the units will be counts versus wavelength. If you need a spectrometer that is calibrated to provide irradiance versus wavelength readings, we offer a Compact Spectroradiometer which is designed for the 380-750nm wavelength range.
A Schlieren test is an optical system that detects changes within a test area medium (air) and records the changes in the form of an image on a screen. The image is formed by refraction and scattering from what is introduced into the test area, which are areas of varying refractive index. A source directs light onto a spherical mirror, which collimates the light and redirects it onto a second identical mirror. The light is then focused onto an included screen. The space between the mirrors is the test area, where the small particles introduced are made visible by the light source and seen as shadows on the screen. Brightness variations on the screen will occur according to changes within the test area. Spherical mirrors are used due to the slight off-axis nature of the set-up. Applications include the determination of refractive index, fluid and air current flow, and flame analysis. Film or video cameras can also be added to the system in place of the imaging screen. Two systems are available with different size F10 mirrors in order to select the test area size that best matches the application.
Please select your shipping country to view the most accurate inventory information, and to determine the correct Edmund Optics sales office for your order.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information