The linear polarizing film is generally manufactured to be 180µm (0.18mm) thick. It is possible to laminate this film onto carrier materials such as TAC, PMMA or glass to obtain different thicknesses depending on customer requirements, i.e. higher stability. Typical available thicknesses are 0.18mm, 0.4mm, 0.75mm, 2mm and 3mm.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information