eo_logo
 
Product added to cart

How can I determine the polarization direction of a polarizing film?

The polarizing direction, also known as the polarization axis, runs parallel to the first mentioned dimension of the polarizing film. For example, a film with the dimension 500mm x 1000mm would have the polarizing direction running parallel to the 500mm side. Square polarizers have the polarizing direction indicated by a sticker on the protective film. In both cases the tolerance is +/- 2°.

這項內容對您是否實用?
 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin
This site is protected by VikingCloud's Trusted Commerce program