Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
Edmund Optics® offers the following types of prisms: right angle, penta, amici roof, Schmidt, dove, littrow, equilateral, trihedral (retroreflection), rhomboid, anamorphic, wedge, light pipe homogenizing rods and compound parabolic concentrators.
Right angle prisms deviate line of sight by 90°.
Penta prisms, half penta prisms, and amici prisms deviate line of sight by 90° without inverting or reverting images; their geometric shapes lend each to different applications.
Schmidt prisms deviate line of sight by 45° while inverting and reverting images.
Dove prisms rotate images by twice the prism rotation angle.
Littrow prisms can be used in two ways: uncoated littrow prisms disperse white light into its component colors and coated littrow prisms deviate line of sight by 60°.
Equilateral prisms disperse white light into its component colors.
Trihedral prisms, or retroreflection prisms, produce 180° beam reflection.
Rhomboid prisms displace the optical axis without inverting images.
Anamorphic prisms expand the incident beam diameter in one direction.
Wedge prisms can be used individually or in pairs: individually, it is used to deviate a laser beam by a set angle, or in pairs, they create an anamorphic prism pair.
Light pipe homogenizing rods homogenize non-uniform light sources. Tapered light pipes also reduce output NA.
Compound parabolic concentrators work similarly to light pipe homogenizing rods; they collect and homogenize light from divergent sources.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information