Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
Edmund Optics offers mirrors with a variety of metallic mirror coatings. Each coating is optimized for a particular spectral region, so care must be used to select a coating that best meets the wavelength, durability, and cost demands of one's application. Protected Aluminum is our most popular mirror coating for applications in the visible and near-Infrared. Enhanced Aluminum is ideal for applications requiring increased reflectance from 400nm-650nm while UV Enhanced Aluminum yields increased reflectance from 250nm-400nm. Protected Gold is effective for applications requiring high reflectance in the near-Infrared and Infrared regions. Protected Silver offers excellent reflectivity in the visible and infrared regions, making it an excellent choice for broadband applications that span multiple spectra. For all these coatings, the theoretical reflectance rises gradually through 10μm.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information