Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
Attenuation is a decrease of light intensity within a fiber, usually due to absorption and scattering losses. This loss of power is measured in decibels (dB) where
dB = 10*log (Pin/Pout)
where:
Pin, Pout are the input and output powers.
The affects of these losses increase with fiber length. The value dB/m measures power lost in dB for every meter of fiber. Edmund Optics' attenuation curves measure the power loss in dB/m for our Communications Grade Optical Fibers and dB/km for our Optical Grade Fibers across the visible spectrum. For example, our 1000 micron diameter Communications Grade Optical Fiber has an attenuation of approximately 0.1dB/m at 600nm. If you were to use a 2-meter fiber, then the total loss would be 0.2 decibels. If we had an input power of 100mW, the output power would then be 95.5mW, resulting in a 5.5% loss. Resultant output power of a fiber, given its attenuation, can be calculated using the equation below:
Pout = Pin * 10-dB/10
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information