Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
"Cross-talk" is when light is scattered from one fiber optic strand to another within a jacketed fiber bundle (or light guide) consisting of several fiber optic strands. It is strongly associated with packing fraction losses. This occurs in both coherent and incoherent fiber bundles. It is typical eliminated by using an absorbing material between the fiber strands or special coating the fiber strands. This is particular noticeable in coherent fibers, where the end faces look almost like a "honeycomb" or grid pattern, because a black absorbing fiber (known as Mural Absorption Fibers, or EMA) is used between the imaging fibers.
"Cross-talk" can also occur when unwanted light from one unjacketed fiber optic strand scatters to another, when they are aligned side-by-side. This is common in communication applications when two fibers transmitting separate signals are in close proximity. Increasing the lateral distance between fiber optic strands and/or using jacketed fibers can eliminate this affect. Our jacketed Fibers Optics do not suffer from cross talk.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information