Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
Optical fibers do not produce beam-like outputs, but rather quickly diverging cones of illumination. They are very good for transmitting light because the fiber core is of a higher index of refraction than the cladding. This index difference not only keeps light in the fiber, but also defines the largest angle of light that the fiber can accept. Due to symmetry principles in fiber optics, the output angle of a fiber is approximately the same as the input angle. The full acceptance angle is defined as the maximum allowable input/output angle for each optical fiber and is directly related to the numerical aperture specification (NA). Our typical acrylic fibers will accept a cone of light approximately 61°, 56° or 35°, which correspond to 0.51, 0.47 and 0.3 NA values respectively. If the input angle, say 30°, is smaller than the acceptance angle, say 61°, then the output angle will still be 30°, not the 61° that one might think. If a fiber is overfilled, the output angle will be slightly less than the acceptance angle due to losses.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information