Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
Concave grating mounts can be monochromatic or spectrographs (polychromatic). Two common concave grating mount configurations are Rowland circle spectrographs and polychromator mounts (also known as flat-field spectrographs). Edmund Optics® offers Zeiss Concave Diffraction Gratings in both configurations.
In a spectrometer using a Rowland circle mount, the entrance slit, illumination source, and the center of the concave grating all lie on the Rowland circle, which has a diameter equal to the tangential radius of the grating curvature. This mount was designed in 1883 by Henry A. Rowland, who was also the first to rule concave gratings of spectroscopy grade quality. Spectra recorded using this mounting configuration are generally free from defocus and primary coma across the wavelength range and spherical aberration is negligible. However, astigmatism can cause issues with the efficiency of the instrument, as a significant fraction of the diffracted light is lost. Therefore, Rowland circle configurations are best suited when a light source with high intensity is used.
Spectrometers with polychromator mounts (flat-field spectrographs) use a fixed arrangement of the entrance slit, concave grating, and flat image plane, which is a linear detector array covering wavelengths of interest. The flat image plane is made possible by changing the groove pattern of the holographic grating by varied line-spacing (VLS) or interferometric methods, which change the focus plane of the grating from a curved shape to a flat surface. This maintains resolution while reducing aberrations such as astigmatism. Instruments with polychromator mounts have a higher light collection efficiency and offer high resolution on flat imaging sensors.
One of the main advantages of using a concave grating in both Rowland circle and polychromator configurations is that, unlike instruments that use plane gratings, no additional focusing optics, such as spherical concave mirrors, are required.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information