Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
A diopter is a measurement of power and has units of inverse meters.
Power (diopters) = 1/EFL where EFL = effective focal length of a lens with units of meters
For a thin lens element, the power is calculated below. Using the magnifying power (MP) of a magnifier or comparator you can calculate the power in diopters.
For the smaller magnifiers:
Power (diopters) = MP/0.25 where EFL is in units of meters
For the larger magnifiers:
Power (diopters) = (MP-1)/0.25 where EFL is in units of meters
Note that this should not be confused with prism diopters. This is also a measure of power, typically used with wedge prisms, that is defined as a 1cm deviation of an input beam at a distance of 1m from the prism.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information