Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
#56-073 Mitutoyo MT-L Accessory Tube Lens is similar in mechanical construction to #56-864 MT-L4 Accessory Tube Lens. In other words, the same basic mounting will work for both.
We offer a #66-027 Mitutoyo MT-L/ MT-L4 C-Mount Adapter to make integration much more simplified. From the C-mount image plane to the MT-L (and MT-L4), you need 176.4mm of space. Factoring in the flange distance of a C-mount camera (17.56mm) and the length of #66-027, you only need 150mm of C-Mount Extension Tubes to fill this space. Since the tube lens does not attach directly to a Mitutoyo objective, #55-743 Mitutoyo to C-Mount 10mm Adapter needs to be attached to the objective (this adapter adds 10mm of length and adapts the M26 thread to a C-thread). This leaves roughly 57mm of space between the tube lens and the objective, which can be filled with extension tubes or other items such as beamsplitters, filters, polarizers, etc.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information