test_cookieUsed to check if the user's browser supports cookies.
最大存储时长: 1 天类别: HTTP Cookie
rc::aThis cookie is used to distinguish between humans and bots. This is beneficial for the website, in order to make valid reports on the use of their website.
最大存储时长: 永久类别: HTML 本地存储
rc::cThis cookie is used to distinguish between humans and bots.
__cf_bm [x3]This cookie is used to distinguish between humans and bots. This is beneficial for the website, in order to make valid reports on the use of their website.
AWSALB [x2]Registers which server-cluster is serving the visitor. This is used in context with load balancing, in order to optimize user experience.
最大存储时长: 7 天类别: HTTP Cookie
AWSALBCORS [x2]Registers which server-cluster is serving the visitor. This is used in context with load balancing, in order to optimize user experience.
_conv_rThis cookie is used as a referral-cookie that stores the visitor’s profile – the cookie is overwritten when the visitor re-enters the website and new information on the visitor is collected and stored.
最大存储时长: 临时类别: HTTP Cookie
_conv_sThis cookie contains an ID string on the current session. This contains non-personal information on what subpages the visitor enters – this information is used to optimize the visitor's experience.
最大存储时长: 1 天类别: HTTP Cookie
_conv_vThis cookie is used to identify the frequency of visits and how long the visitor is on the website. The cookie is also used to determine how many and which subpages the visitor visits on a website – this information can be used by the website to optimize the domain and its subpages.
conv_randThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
最大存储时长: 永久类别: HTML 本地存储
_conv_sptestThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
_ga [x2]Used to send data to Google Analytics about the visitor's device and behavior. Tracks the visitor across devices and marketing channels.
最大存储时长: 25 月类别: HTTP Cookie
_ga_# [x2]Used to send data to Google Analytics about the visitor's device and behavior. Tracks the visitor across devices and marketing channels.
最大存储时长: 25 月类别: HTTP Cookie
_gcl_au [x2]Used by Google AdSense for experimenting with advertisement efficiency across websites using their services.
最大存储时长: 3 月类别: HTTP Cookie
IDE待定
最大存储时长: 400 天类别: HTTP Cookie
NIDRegisters a unique ID that identifies a returning user's device. The ID is used for targeted ads.
最大存储时长: 6 月类别: HTTP Cookie
pagead/1p-user-list/#Tracks if the user has shown interest in specific products or events across multiple websites and detects how the user navigates between sites. This is used for measurement of advertisement efforts and facilitates payment of referral-fees between websites.
The most common adhesive we use for bonding our prisms is Norland NOA61. It is low-shrink (so the pieces won't move as it cures) and has excellent bonding strength for glass-to-glass. The adhesive is UV cured, so you'll need a UV source to make it stick. Once cured the adhesive is opaque to UV light but still works great if you are going to use the glued prism pair for visible or NIR applications, in other words, you can expect high transmission from 400 - 2000nm.
Yes. UV adhesives are optimized to cure under UV light. UV adhesives absorb UV light and pass the visible and IR portions of the spectrum. However, since sunlight and most room lights also emit in the UV, the adhesives will cure under these conditions. Please note that initial and full cure times will be considerably longer, because there will be less energy spread over a larger area then when compared to a UV curing light source.
The choice of adhesive depends upon your application. Adhesives can be classified into two groups: optically opaque adhesives and optically transparent adhesives.
Optically opaque adhesives are used when light is not going to be transmitted through the adhesive, such as when bonding a mirror to an aluminum mount. Milbond and Loctite® are two such adhesives. Milbond adhesive, for example, uses two bonding agents that, when combined, create the adhesive. There is also a decementing agent available for Milbond that allows the adhesive to be removed when necessary. These type of adhesives do not require UV light in order to cure.
Optically transparent adhesives allow light to transmit through and are commonly used to bond lenses together. The Norland and Summers lines are two such adhesives. When cured with a UV light source, the adhesive has a defined index of refraction which we list under the specifications of each adhesive. Please note that UV adhesives such as Summers and Norland do not come with decementing agents and are very difficult to break the adhesion once cured.
Light Absorbing Black-Out Material is not tested for vacuum environments and the adhesive is likely to outgas in vacuum environments.
Please select your shipping country to view the most accurate inventory information, and to determine the correct Edmund Optics sales office for your order.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information