Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
Microscope objectives come in many different designs. Three of the most common are achromatic, semi-plan and plan. In an achromatic objective, which is the most common type, there is one achromatic lens. Achromatic objectives correct for color and have a flat field in about the center 65% of the image. This is not to say that the outer 35% of the image will be blurry- this just means that if there are aberrations, they occur in the outer 35% of the image. A semi-plan, or semi-planar objective, is an intermediate between the achromatic and the plan objective. Semi-plan (sometimes called micro-plan as well) objectives have an 80% flat field. A plan (or planar) objective corrects better for color and spherical aberration than either the semi-plan or the achromatic objective. Plan objectives have a flat field about the center 95% of the image. While plan objectives give you flatter fields than achromatic objectives, they also have a higher price.
Eyepieces for both microscopes and telescopes come in varying optical designs. The major differences between the three microscope eyepiece designs we carry is listed below:
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information