Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
An in-line microscope introduces illumination into the system before the objective and aligns it with the optical axis. The "in-line" name actually refers to the type of illumination and is also known by other names such as axial, co-axial, through-the-objective, vertical, and incident brightfield. The clear difference from other types of illumination is that in this case the light is transmitted through the objective. An infinity-corrected system is used for this type of microscope. Since the light between the objective and secondary lens is collimated, the separation between these lenses can be adjusted to accept a beamsplitter that will introduce horizontally aligned input light and redirect it vertically down to the objective. This type of illumination is very efficient for high power objectives that need to evenly illuminate an opaque object, such as a semiconductor wafer. Since this type of system is very sensitive to mounting with objective powers 20X and higher, we recommend using a vibration isolation platform. For proper focusing, a rack and pinion movement is always suggested for the system.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information