Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
Under most conditions, a laser beam cannot be seen traveling through the air. Since our eyes are essentially light collectors, we can only see light that enters the eye and is imaged onto our retina. When a laser beam encounters dust, mist, or smoke, some fraction of the light is scattered in the direction of the viewer's eyes and therefore becomes visible. Since these particles are rather small and will not stop the entire beam, all the tiny reflections make the beam look solid or continuous. This is why the beam appears to slowly fade as the dust (or scattering medium) dissipates. In the absence of any type of scattering medium, the beam will only be visible as a spot when it reaches its target and energy reflects back to the viewer. This principle can easily be demonstrated by using a flashlight on a dark night: if it is foggy, you can see the cone of light coming from the flashlight; if it is not foggy, you can only see the light as a spot at its target. If you see something that appears to contradict this concept, it is usually just 'movie magic'.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information