eo_logo
 
Product added to cart

Edmund Optics®

知識中心

 由我們 240 多位全球工程師創建且經過驗證的可信任技術資源庫。

Filter
Search Results for: UV and IR Windows | 紫外或紅外窗鏡 (160)

紫外雷射

A new generation of small, cost-effective, CW ultraviolet (UV) lasers allows more applications to move to UV wavelengths for increased power and precision.

現在查看 添加內容至保存

在紅外應用中使用彎月透鏡的優勢

Meniscus lenses offer superior performance compared to plano convex lenses in IR applications. Find out the benefits of using a meniscus lens at Edmund Optics.

現在查看 添加內容至保存

極紫外線光學元件

Pushing Optics to the Extreme

現在查看 添加內容至保存

選擇正確的紅外線(IR)正確材料

Using an Infrared Application? Discover the importance of choosing the right material and comparisons of each at Edmund Optics.

現在查看 添加內容至保存

使用紅外線光譜進行假藥檢測

紅外線光譜用於檢測假藥中的有害化學物質,這對於在現場或實驗室應對鴉片類藥物危機至關重要。

現在查看 添加內容至保存

未來的顯微鏡物鏡

Advances in Microscopy Tackle the Challenges of the Future

現在查看 添加內容至保存

半導體超級反射鏡

Semiconductor supermirrors offer high reflectivity and outperform many IR mirrors on the market. Learn more about these new supermirrors at Edmund Optics.

現在查看 添加內容至保存

下一代球面透鏡

Traditional spherical lenses are evolving due to the increasing demands of applications. Learn about the future of spherical lenses at Edmund Optics.

現在查看 添加內容至保存

反射鏡金屬鍍膜

Want to learn more about metallic mirror coatings? Find information about standard and custom metallic mirror coatings that are available at Edmund Optics.

現在查看 添加內容至保存

菲涅耳透鏡的優點

Fresnel lenses come in different sizes and can be used in a variety of applications. Read more about the theory, manufacturing, and application use at Edmund Optics.

現在查看 添加內容至保存

成像鏡頭的強化設計

在嚴苛的環境中擁有應用程式嗎?了解愛特蒙特光學的不同類型的加固:工業、入口保護和穩定性。

現在查看 添加內容至保存

為什麼使用消色差透鏡?

想知道為什麼應該使用消色差透鏡嗎?在愛特蒙特光學了解有關消色差透鏡的更多信息,包括解剖結構、顯著特徵等

現在查看 添加內容至保存

鏡頭的解剖結構

熟悉成像鏡頭組件的關鍵組件及其運作原理。

現在查看 添加內容至保存

盡可能減少超快系統的熱透鏡效應

Specialized coatings can minimize thermal lensing in ultrafast laser systems, which are particularly susceptible to detrimental thermal effects.

現在查看 添加內容至保存

非球面透鏡的製造方式

愛特蒙特光學® 在每天 24 小時運作的非球面製造單元中每月生產數千個精密非球面透鏡。

現在查看 添加內容至保存

加固成像鏡頭

Not all ruggedized imaging lenses feature the same type of ruggedization. Learn about the advantages and disadvantages of each type at Edmund Optics.

現在查看 添加內容至保存

鑽石車削離軸拋物面反射鏡的粗糙度

Learn about spatial frequency errors and surface roughness of Single Point Diamond Turned off-axis parabolic mirrors at Edmund Optics.

現在查看 添加內容至保存

桿式反射鏡

Mounting flat mirrors by their edges in a kinematic mount imparts stress onto the mirror surface. This results in distortion and reduced quality of the reflected wavefront, which is especially noticeable when using high-quality mirrors. Stemmed mirrors, on the other hand, are mounted from a smaller diameter “stem” protruding from the back of the mirror, resulting in significantly reduced stress on the mirror surface, high stability, and cost reduction and can be used as a replacement for a more expensive and complex kinematic mount and a conventional mirror.

現在查看 添加內容至保存

MTF 曲線和鏡頭性能

透過直接比較相關的調變傳遞函數 (MTF) 曲線來探索成像鏡頭表現的差異。

現在查看 添加內容至保存

用於成像的液態鏡頭

Quickly Autofocus and Overcome Depth of Field Limitations

現在查看 添加內容至保存

傳感器和鏡頭

成像鏡頭和感光元件配對時必須特別注意。

現在查看 添加內容至保存

雷射擴束鏡

雷射擴束鏡對於降低功率密度、最小化遠距離光束直徑以及最小化聚焦雷射光斑尺寸至關重要。

現在查看 添加內容至保存

組裝液態鏡頭 Cx 系列鏡頭

進一步瞭解如何將液態鏡頭插入 TECHSPEC® 液態鏡頭 Cx 系列定焦鏡頭組件。

現在查看 添加內容至保存

E 系列動態光學反射鏡調整組件

E 系列運動光學安裝座為實驗室使用、原型設計和系統整合等應用提供高價值和基本功能

現在查看 添加內容至保存

遠心照明:機器視覺應用不可或缺的技術

您認為機器視覺應用不需要遠心照明嗎?了解愛特蒙特光學為何需要遠心照明。

現在查看 添加內容至保存

適用於雷射應用的反射式光學產品

Beam Conditioning Optics for UV, IR, and Broadband Lasers

現在查看 添加內容至保存

基礎鏡頭選型

要確定哪種成像鏡頭適合系統,了解所使用成像系統的參數非常重要。在愛特蒙特光學了解更多。

現在查看 添加內容至保存

遠心鏡頭大小控制

在小放大倍率下,遠心鏡頭可能變得相當大且重,因為這種放大倍率需要大的前置光學。在愛特蒙特光學了解更多。

現在查看 添加內容至保存

了解顯微物鏡

想了解更多關於顯微物鏡的知識嗎?了解愛特蒙特光學用於建立顯微物鏡的不同組件、關鍵概念和規格。

現在查看 添加內容至保存

液態透鏡基礎原理

使用液體鏡頭可以增強成像鏡頭的性能。在愛特蒙特光學了解更多。

現在查看 添加內容至保存
 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin
This site is protected by VikingCloud's Trusted Commerce program