Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
Edmund Optics® (EO), the premier provider of optical components, will unveil their new TECHSPEC® Variable Beam Expanders at the CLEO show in San Jose, CA. These versatile beam expanders offer continuous magnification for high power laser applications where magnification changes may be required, including prototyping or research and development.
¼λ transmitted wavefront
Edmund Optics’ TECHSPEC Variable Beam Expanders provide 1-3X and 2-8X continuous magnification. These Galilean designs feature a guaranteed ¼λ transmitted wavefront. High laser damage threshold anti-reflective (AR) coatings ensure maximum transmittance, while minimizing ghost reflections.
Non-Rotating Optics Design
TECHSPEC Variable Beam Expanders use non-rotating internal translation and focusing mechanisms to continuously adjust magnification and laser divergence without any effect on the overall housing length. The compact design eliminates the need to make system accommodations for changes in length and simplifies system integration. It easily adjusts for laser beam divergence.
Continuous Magnifications of 1-3X and 2-8X are available
TECHSPEC Variable Beam Expanders are available in two different magnification ranges – from 1-3X or 2-8X – for 532 nm, 1064 nm, or broadband visible wavelengths. Custom fixed magnification requirements can also be accommodated.
Visit http://www.edmundoptics.com/vari-beam to learn more about the TECHSPEC Variable Beam Expanders.
Please stop by Booth #2007 to see the TECHSPEC Variable Beam Expanders at CLEO, the Conference on Lasers and Electro-Optics, June 10-12, at the San Jose Convention Center, San Jose, CA.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information