Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
我们不使用这种类别的 cookie
Edmund Optics® (EO), the premier provider of optical components, announces the TECHSPEC® Nd:YAG Harmonic Separators. These beamsplitters are used to separate the common harmonic wavelengths of an Nd:YAG laser. The precision mirrors are designed for a wide range of demanding Nd:YAG laser applications.
TECHSPEC® Nd:YAG Harmonic Separators are dichroic mirrors used for separating the harmonic, frequency-doubled beam from the pump beam, which is often outside the laser resonator. The frequency doubled light is reflected to nearly 100%, while most of the pump light is transmitted.
TECHSPEC® Nd:YAG Harmonic Separators have a beamsplitter coating on the first surface, which reflects at least one wavelength and transmits another. The beamsplitter coating features greater than 95% transmission. The second surface has an anti-reflective coating to minimize losses from reflection. Designed for integration at 45° angle of incidence, the harmonic separators are manufactured using a precision λ/10 fused silica substrate that offers excellent optical and thermal performance and stability, along with a surface quality of 10-5. The RoHS compliant mirrors have a thickness of 6.35 ±0.20mm, plate construction, and a clear aperture of greater than 85%.
TECHSPEC® Nd:YAG Harmonic Separators are available in multiple wavelength configurations for maximum system design flexibility. Fourteen models offer diameters of 12.70mm and 25.40mm at common Nd:YAG wavelengths of 1064nm, 532nm, 355nm and 266nm. TECHSPEC® Nd:YAG Harmonic Separators are in-stock and available for immediate delivery.
About Edmund Optics:
Edmund Optics® is a leading supplier of optics, imaging, and photonics technology for the Life Sciences, Biomedical, Semiconductor, R&D, and Defense markets around the globe. Edmund Optics designs and manufactures a wide array of multi-element lenses, lens coatings, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of both stock and custom products. Edmund Optics’ state-of-the-art manufacturing capabilities, combined with its global distribution network, has earned it the position of the world’s largest supplier of off-the-shelf optical components. Customers can purchase items by calling 1-800-363-1992, via the catalog or the website at www.edmundoptics.com.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information