Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
我们不使用这种类别的 cookie
Edmund Optics®, a global manufacturer and solutions provider of optical technology, is proud to announce that its UAV Series Fixed Focal Length Lenses have won the Silver-Level 2024 Vision Systems Design (VSD) Innovators Award. These lenses are compact, lightweight, and high-resolution, optimized for use on autonomous vehicles and drones.
The UAV Series Lenses are athermalized for wide temperature ranges and ruggedized to maintain performance throughout shocks and vibrations, making them ideal for drone mapping and surveying, aerial imaging, and photogrammetry applications.
Normally, lenses need to grow in size, weight, and complexity in order to accommodate higher resolutions, but the UAV Series Lenses maintain a compact size while achieving up to 24.4 megapixel resolution on 2.74µm pixel size sensors. They are tailored for new, high-resolution image sensors like the 4th-generation Sony Pregius 1.2” IMX530 and IMX540 sensors.
Locking focus and iris rings in the UAV Series Lenses prevent unwanted adjustments during use. These lenses are also optimized for long working distances, as these mobile robots often look at objects further away than those on a factory floor. Extra care was also taken to minimize stray light throughout the lens assemblies, which is critical because the conditions found in robotics environments are much less controlled than those on a factory floor.
Other available lenses that can match the 24.4 megapixel resolution of the UAV Series Fixed Focal Length Lenses from Edmund Optics are much larger and heavier, making them impractical for mobile applications. The UAV series lenses use streamlined mechanics and tight tolerances attained through advanced assembly techniques to achieve both a small form factor and high resolution.
The UAV Series Fixed Focal Length Lenses from Edmund Optics are available in 16mm, 25mm, and 35mm focal lengths and are available off-the-shelf for immediate shipping.
More details can be found here.
About Edmund Optics:
Edmund Optics® is a leading, global provider of optical technology solutions that has served markets ranging from life sciences, to industrial inspection, to materials processing since 1942. The company services customers through two distinct offerings: a marketplace that serves as a one-stop shop for the best brands and products in optics and photonics; and custom and volume manufacturing of precision optical and imaging components and systems. In-house application expertise, design, and research and development collaborate to discover creative solutions to customers’ optical challenges. The company employs 1,250+ employees across 18 global locations and continues to expand. Customers can learn more, speak to an engineer, or purchase items through our website at www.edmundoptics.com.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information